Technical FAQs

Ask a Question

What is the maximum current allowed on a C-Bus network.

The maximum current allowed on a C-Bus network is 2000mA, this can be provided by any combination of available power supplies, either inbuilt to output units (200mA), or on the standalone power supply (5500PS, 350mA).
Was this helpful?
What can we do to improve the information ?