Technical FAQs

Ask a Question

At what value of input for BMXSAI0410 channels shows current out of range alarm.

The BMXSAI0410 module detects a cut wire condition and reports it as a current out of range condition at current value less than 3.75 mA or greater than 20.75 mA.
Was this helpful?
What can we do to improve the information ?