Technical FAQs

Ask a Question

How to detect current out of range alarm in BMXSAI0410.

The BMXSAI0410 module detects a cut wire condition and reports it as a current out of range condition at current value less than 3.75 mA or greater than 20.75 mA by setting the OOR element of the T_U_ANA_SIS_CH_IN structure to “1”.
Was this helpful?
What can we do to improve the information ?