Technical FAQs

Ask a Question

Which wiring connector can be used with BMXSRA0405 digital relay output module.

The following Schneider Electric 20-point terminal blocks to fit the 20 pin connector on the front of the module:
 
1. screw clamp terminal block BMXFTB2010
2. age clamp terminal block BMXFTB2000
3. spring type terminal block BMXFTB2020
 
NOTE: Terminal blocks can be removed only when power to the module is OFF.
Was this helpful?
What can we do to improve the information ?