Technical FAQs

Ask a Question

What is the Time stamp resolution between 2 events on different source modules as BMXERT1604T.

Below are the time stamp value for BMXERT1604T:
 
1. 2ms with IRIG-B 004/5/6/7 time code (GPS)
2. 4ms with DCF77 time code
 
Note: Time Stamp resolution is given if each BMXERT1604T module is supplied with the same time source.
Was this helpful?
What can we do to improve the information ?