Technical FAQs

Ask a Question

Does ATV610 has MOV or RC connected to ground for each phase via body earth. If yes, any jumper to disconnect them.

ATV610 have RC connect to the ground, and it can be disconnected by IT jumper (the integrated EMC filter must be disconnected).
 
Was this helpful?
What can we do to improve the information ?