Technical FAQs

Ask a Question

When DC injection is turned on via Digital Input on ATV630 drive, is DC injection current supplied to the motor constantly regardless of time.

DCI function is assigned to Dix
=>So, when Dix is high
=>then DC injection current is supplied to the motor constantly regardless of time.


 
Was this helpful?
What can we do to improve the information ?