Technical FAQs

Ask a Question

Is it possible to Use Line choke and DC choke both on ATV71/ATV61 Drives.

Line choke and DC choke must not be used both because the drop voltage across them would be too high and the maximum output torque can't be guaranteed on the motor.
 
Was this helpful?
What can we do to improve the information ?