Technical FAQs

Ask a Question

What is the voltage drop at 10 meter for 24VDC for XS630B1PAL10 and XS630B1MAL10.

For XS630B1PAL10 and XS630B1MAL10, using electrical cable with wires 0.34mm2, in 24Vdc voltage, 10m length, copper wire, load 3W, the voltage drop is < 0.1V (or <0.5%).


 
Was this helpful?
What can we do to improve the information ?