Technical FAQs

Ask a Question

Unable to create or open a project in Unity Pro XL v13.0 in Windows 10 Home 64-bits OS

Unity Pro v13.0 is only tested & validated for below OS:

 Microsoft Windows 7 Professional 32-bit / 64-bit
 Microsoft Windows 8.1 Pro 32-bit / 64-bit
 Microsoft Windows 10 Pro 32-bit / 64-bit
 Microsoft Windows Server 2008 R2 Standard 64-bit
 Microsoft Windows Server 2012 R2 Standard 64-bit
Was this helpful?
What can we do to improve the information ?