Technical FAQs

Ask a Question

when Launching UPV13.1 after successful installation, An error message came out ( Error initializing the programming unit (STMSDK COM object initialization): Unexpected exception (memory allocation,)

Open a command prompt as an administrator and move to the installation path and type : regsvr32 stmsdk.dll

If you get the successful Registration as shown below, It means that the registration is done without any errors. You have to run Unity to test..



 
Was this helpful?
What can we do to improve the information ?