Technical FAQs

Ask a Question

What is the maximum cable length permissible according to baudrate of profibus?

The maximum cable length depends on the transmission speed and cable type. The
specified cable length can be increased using the repeaters. The use of more than 3
repeaters in series is not recommended.
Baudrate (kbps)   9.6     19.2    93.75    187.5    500    1500      3000-12000
Length A (m)       1200   1200   1200     1000     400     200           100
Was this helpful?
What can we do to improve the information ?