Search FAQs
What is the default ip address of PTQ-PDPMV1 ethernet port ?
The PTQ-PDPMV1 module is equipped to use an Ethernet connection using the following defaults:
My_ip: 192.168.0.100
Netmask: 255.255.255.0
Gateway: 192.168.0.1
For HSBY units the remote (passive) Master module Ethernet connection is always Primary IP plus 1. For example, Primary IP = 192.168.0.100, Standby module IP = 192.168.0.101.
This setting is not configurable: the module's firmware automatically sets the IP address of the remote (passive) Master.
My_ip: 192.168.0.100
Netmask: 255.255.255.0
Gateway: 192.168.0.1
For HSBY units the remote (passive) Master module Ethernet connection is always Primary IP plus 1. For example, Primary IP = 192.168.0.100, Standby module IP = 192.168.0.101.
This setting is not configurable: the module's firmware automatically sets the IP address of the remote (passive) Master.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: