Technical FAQs

Ask a Question

What is the starting address of input/output image for PTQ-PDPMV1 module ?

The starting address for the input image is 1000 and for the output image is 3000.
Was this helpful?
What can we do to improve the information ?