Technical FAQs

Ask a Question

How can I add the Magelis HMIGXO in Vijeo Designer?

Issue:
The Magelis HMIGXO series are only available for the Asian Market. However, sometimes a machine built by an Asian machine builder may sell a unit to a customer in another part of the world and it might be neccesary to update the application with Vijeo Designer if the equipment was shipped to a different country,

Product Line:
HMIGXO3501
HMIGXO3502
HMIGXO5502

Environment:
Vijeo Designer V6.2

Resolution:

To enable the GXO target in Vijeo Designer V6.2
1. Launch Vijeo Designer
2. Go to Help\About\License\Upgrade. 
3. Enter the Upgrade Reference Number VJDHTGTGX and press OK. 

Note: Vijeo Designer must be registered.
Was this helpful?
What can we do to improve the information ?