Technical FAQs

Ask a Question

Does ATV930 drives developed to meet the requirements of directives regarding protection of the environment.

The Altivar Process drive has been developed to meet the requirements of directives regarding protection of the environment and anticipate future changes in regulations:---
-RoHS-2 (1)
-REACh (2) + Solution for REACh Substitute It Now (halogen-free wiring and
 plastics)
-PEP (Product Environmental Profile) eco-passport Program for reducing the
 carbon footprint and conserving raw materials
-EoLI (End of Life Instruction) (3)
 More than 70% recyclable materials (new ruling)
-Efficient energy management: 30% reduction in consumption

 where =>
(1) European directive 2002/95/EC Restriction Of Hazardous Substances (applicable in 2016)
(2) European regulation 1907/2006
(3) According to IEC 62635 Enhanced Guidelines
 
 
 
 
Was this helpful?
What can we do to improve the information ?