Technical FAQs

Ask a Question

What are the Fieldbus protocols integrated on ATV930 drives.

EtherNet/IP and Modbus/TCP Dual port and Modbus serial link:--
- Standard Modbus and Ethernet protocols
- Connection of configuration and runtime tools
-  Control and supervision of the Altivar Process in process architectures
(controllers, SCADA, HMIs, etc.) in industrial networks (read/write data)
- Diagnostic, supervision, and fieldbus management functions
 
Ethernet services:--
-SNMP, SNTP, BootP & DHCP, IP v6, cybersecurity services, FDR
-Open Ethernet topologies
 
Was this helpful?
What can we do to improve the information ?