Technical FAQs

Ask a Question

What is CPR (E23) fault on Altivar AFE.

ASIC on the line control cannot be initialized.
An internal failure occurred.
Remedy: Shut down mains supply, wait for complete discharge of DC link (LED 1) and switch on
again. If the fault is still present, the control block has to be exchanged.
 
Was this helpful?
What can we do to improve the information ?