Technical FAQs

Ask a Question

How can we save a recording using the trending tool in unity pro?

To save a recording in trending tool:
Step
Action
1
Use the Save trend command from the Services menu. If this is the first time that the document has been saved, Trending Tool will open the standard Windows Save as dialog box.
2
In the dialog box, type a name for the recording and select the location where you want to save the file. Click on the
OK button to close the dialog box and save the document. 
 
Was this helpful?
What can we do to improve the information ?