Technical FAQs

Ask a Question

How can we open a previously saved recording (.MAP file) using the trending tool in unity pro?

To open a previously saved recording or configuration in Trending Tool:
Step
Action
1
Use the Open trend command from the Services menu. This command opens the standard Windows Open dialog box.
2
In the dialog box, select the required file and click on the OK button to open a Trending Tool recording window containing the selected recording. 
 
Was this helpful?
What can we do to improve the information ?