Technical FAQs

Ask a Question

Are the 9080 Power Distribution Blocks available with ring termination?

Issue:
9080 Power Distribution Blocks Ring Tongue Terminal

Product Line:
Class 9080, Type LB Power Distribution Blocks

Environment:
NEMA Type LB Power Distribution Blocks

Resolution:
Ring terminals are not available.
Was this helpful?
What can we do to improve the information ?