Browse FAQs

Why does F010 fault occurs in ATV310 Drive

Published date: 31 July 2019

Name of fault :- Over current 

    Possible causes:-

    • Parameters in the Motor control menu are not correct
    • Inertia or load too high
    • Mechanical locking

    Remedy :-
    
   • Check the motor control parameters.
   • Check the size of the motor/drive/load.
   • Check the state of the mechanism.
   • Connect line motor chokes.
   • Reduce the Switching frequency range
   • Check the ground connection of drive, motor cable and motor insulation.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.