Technical FAQs

Ask a Question

How to monitor RAM battery voltage onto Scadapack E devices?

To monitor the RAM battery voltage onto the Scadapack E devices the firmware version must be at least 8.14.6 or greater.

Used Analog System Point 50061

This analog system point measures the available battery voltage. It is useful for measuring the operating environment of the RTU and returns a floating point value in the range 0...32.767 Vdc.

·Use the system point directly by assigning a point of this point number (50061) in the RTU database.

·Read the system point into a user-created SCADAPack Workbench or ISaGRAF 3 Workbench application as an integer or real variable from an input board connection.

Was this helpful?
What can we do to improve the information ?