Browse FAQs

How can the minimum or maximum current values be found on the PM8000 front panel?

Published date: 01 April 2019

Issue
How can the minimum or maximum current values be found on the PM8000 front panel?
 
Product Line
PM8000
 
Environment
Metering & Power Monitoring
 
Resolution
From the meter front panel:
  • Press ‘Home’ to display the menu
  • Press ‘Up’ or ‘Down’ until Basic Readings is highlighting
  • Press ‘Check mark’ to view the basic readings screens
  • Press ‘Down’ until Current is highlighted
  • Press the ‘Check mark’ to view the current screens
  • Press the ‘+’ to show a list of additional screens
  • Choose the additional screen (I Average, I Min (Ia Ib Ic), I Min (I4), I Max (Ia Ib Ic), or I Max (I4)) to view the minimum or maximum current values

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.