Technical FAQs

Ask a Question

Is the reset button on the HMI used for fault reset while in terminal mode in ATV71.

Reset button on the HMI is not used for fault reset while in terminal mode.
Use the Logical input assignment in the menu -> Fault Management->Fault Reset.
Was this helpful?
What can we do to improve the information ?