Technical FAQs

Ask a Question

ATV630 Sensorless flow estimation can it maintain a constant pressure?

Issue:
Can the ATV630 drive be configured to maintain a  constant pressure, using the Sensorless flow estimation function?
 
Product Line:
ATV630
 
Environment:
All serial numbers
 
Cause:
No external PI control
 
Resolution:
No, it is not possible to maintain constant pressure control with Sensorless Flow Estimation.
Was this helpful?
What can we do to improve the information ?