Technical FAQs

Ask a Question

What is the dielectric strength value available in BMXDDI3202K?

The Dielectric strength value of BMXDDI3202K
    
    500 V DC 1 minute, between group of channels
    1500 V AC at 50/60 Hz 1 minute, primary/secondary
Was this helpful?
What can we do to improve the information ?