Browse FAQs

Compare 2 SoMove LXM32 configurations

Published date: 15 May 2019

Issue:
How to find the difference between 2 SoMove LXM32 configurations

Product Line:
SoMove, LXM32

Resolution:
1- First, make a SoMove file with default values (FSU) and then compare with the SoMove file that has the edited parameters.
2- Both configuration files will be displayed on the screen and the highlighted values are those parameters that are different

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.