Browse FAQs

​​​​​​​Does the ATV320 have 2 ramps functionality?

Published date: 12 April 2019

Issue:
Can I do dual ramps with the ATV320 drives?

Product Line:
ATV320

Environment:
All serial numbers 

Cause:
Application requirement 

Resolution:
Yes, There is a second acceleration ramp option, ACC2 (ranges from 0.00 - 6,000 seconds) 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.