Technical FAQs

Ask a Question

Can I get a second analog output on the ATV340 drive?

Issue:   
Can I get a second analog output on the ATV340 drive?

Product Line:   
ATV340
 
Environment:  
 All

Cause:   
Customer needs a second analog output. Looking the a I/O expansion module
 
Resolution:   
No. There are only 2 I/O expansion modules for the ATV340 drive. The VW3A3203 has 6 digital inputs, 2 digital outputs, and 2 analog inputs, and the VW3A3204 has 3 relay outputs.
 
Was this helpful?
What can we do to improve the information ?