Technical FAQs

Ask a Question

How to monitor drive run time on the ATV212 drive?

Issue:
How to monitor drive run time on the ATV212 drive?

Product Line:
Altivar ATV212

Environment
All serial numbers

Cause:
Customer wanted to monitor the drive run time in the ATV212 drive.

Resolution:
The drive run time of the ATV212 is under the monitor menu or Fr-F.  Using the integral keypad, push the MODE button until you see Fr-F.  Do not push Enter, scroll down until you see t0.12.  In this case, t0.12 is equal to 12 hours.  See the attachment below for more details.



 
Was this helpful?
What can we do to improve the information ?