Technical FAQs

Ask a Question

Does the ATV212 drive have 10Vdc internal power supply?

Issue:
Does the ATV212 drive have 10Vdc internal power supply?

Producl Line:
Altivar ATV212

Environment:
All

Cause:
Customer wanted to know if drive has 10Vdc so that he can test VIA 0-10V signal on the drive without using his 0-10Vdc analog signal from PLC.

Resolution:
The internal power supply on the ATV212 is at terminal PP.
Was this helpful?
What can we do to improve the information ?