Technical FAQs

Ask a Question

Is cable included on XMLG010D21 & XMLG001D21.

Cable is not included on XMLG010D21 & XMLG001D21.
On XMLG010D21 & XMLG001D21; its (XML G***D21 ) Electrical connection have M12, 3-pin male.

Following are the suitable female connectors, including pre-wired versions, -
1. Pre-wired M12, straight, female connectors 2 m - XZ CP1141L2
2. Pre-wired M12, straight, female connectors 5 m - XZ CP1141L5
3. Pre-wired M12, straight, female connectors 10 m - XZ CP1141L10
4. Pre-wired M12, elbowed, female connectors 2m - XZ CP1241L2
5. Pre-wired M12, elbowed, female connectors 5m - XZ CP1241L5
6. Pre-wired M12, elbowed, female connectors 10m- XZ CP1241L10

 
Was this helpful?
What can we do to improve the information ?