Technical FAQs

Ask a Question

Do we have Line Choke for ATV340D30N4E drive.

For drives above 30 kW, ATV340D30N4E...D75N4E, a DC choke is integrated, so an extra line choke is not required.
Note: External line chokes are not required for variable speed drives ATV340D30...D75N4E,
in which integrated DC chokes serve for the same purpose.

 
Was this helpful?
What can we do to improve the information ?