Technical FAQs

Ask a Question

Is it possible to use ZBY9140T, ZBY9130T, ZBY9330T & ZBY9230T legend with metal guard ZBZ160*.

it is not possible to use ZBY9140T, ZBY9130T, ZBY9330T & ZBY9230Twith metal guard ZBZ160*.
However; following legend part numbers can be used with ZBZ160*:
ZBY9140M, ZBY9130M, ZBY9330M, ZBY9430M, ZBY9430M, ZBY9530M, ZBY9630M, ZBY9730M & ZBY9830M
Refer to catalog (page 105 highlighted in red square).
Was this helpful?
What can we do to improve the information ?