Technical FAQs

Ask a Question

How is the memory management of LMC078 controller?

The RAM size is 512 MBytes and used for system variable(%I, %Q, %M) and also for user symbols, variables, application, and libraries.
This should be always enough for each kind of customer application and there should be no need to test it.
The NVRAM size is only 128 KBytes and used retained and/or persistent retained variables.
This means there is a limit of around 32000 persistent retained variable from datatype REAL.
Was this helpful?
What can we do to improve the information ?