Technical FAQs

Ask a Question

What is the drop out and pickup voltage of RXM4AB1U7 relay?

“Drop-out voltage” and “Pick-up voltage” specifications. 
Drop-out voltage = 36Vac 
(This is the value which all contacts must return to their de-energized position) 
Pick-up voltage = 192Vac 
(This is the value which all contacts must switch the contacts "on" or energized) 
Was this helpful?
What can we do to improve the information ?