Technical FAQs

Ask a Question

We observed that AOA local projects stop working after 15 days in AOA v2.3

This is normal behavior in AOA v 2.3 . 

Locally copied projects are only valid for 15 days after the project was last modified in the EcoStruxure Augmented Operator Advisor Builder. 

To solve this issue, follow the below steps: 

1. Make some small changes in project in AOA builder. 
2. Build project 
3. Download project 
4. unzip downloaded project 
5. Paste the unzipped project folder in local folder of Ipad .follow below location for path of local folder: 

- On an Android tablet: ..\Android\data\com.schneiderelectric.AugmentedOperator\Local 

- On an IOS tablet: ..\Apps\Ecostruxure Augmented Operator Advisor\Documents\Local 

- On a Windows tablet: C:\ProgramData\Schneider Electric\Ecostruxure Augmented Operator Advisor\Local 
Was this helpful?
What can we do to improve the information ?