Technical FAQs

Ask a Question

How to print a SoMachine project?

Issue:
How to print a SoMachine project?

Product Line:
SoMachine

Resolution:
Possible reasons of the A320 error are:
1. Higher amount of friction in application that is on this motor - check the mechanical if there is some blockage, check bearing.
2. Gearbox attached on the motor has higher friction because it lost lubrication
Was this helpful?
What can we do to improve the information ?