Technical FAQs

Ask a Question

How is the ATV212 set for RUN/STOP on the terminals and UP/DOWN arrows for the speed reference?

Issue:
How is the ATV212 set for RUN/STOP on the terminals and UP/DOWN arrows for the speed reference?

Product Line:
Altivar 212

Environment:
All models

Cause:
Customer needs to use terminals for Start/Stop and Arrows on the faceplate of drive, for speed reference

Resolution:
There is no option for that configuration.
Was this helpful?
What can we do to improve the information ?