Technical FAQs

Ask a Question

Vijeo Designer - Can a Virtual Drive from a Virtual Machine be used to transfer license rights via removable media?

Issue
I wish to transfer a license from an existing licensed copy of Vijeo Designer to a Virtual Machine.
Can a Virtual Machine's Virtual Drive be used to transfer license rights via removable media?

Product Line
Vijeo Designer V6.x

Environment
Windows 7 or Windows 10 PC,  Windows 7 or Windows 10 Virtual Machine

Resolution
No. It is not possible to use a Virtual Drive on a Virtual Machine to transfer license rights using the Vijeo Designer License Manager. A physical USB memory stick must be used.
Was this helpful?
What can we do to improve the information ?