Technical FAQs

Ask a Question

What to check if the touch screen of an HMIG5U/HMIG5U2 is not responding.

Issue:
What to check if the touch screen of an HMIG5U/HMIG5U2 is not responding.

Product Line:
HMIG5U, HMIG5U2, iPC

Resolution:
If the touch screen of your HMIG5U or HMG5U2 is not responding to your touch, plug in a keyboard and mouse and navigate to the Windows Services settings by typing "services" in the Start Menu. 

Upon opening the Windows Component Services dialog, click on "Service (Local)" and find the "TabletPCInputService" service. Ensure that this service is setup to run Automatically and is currently runnning.

If the service is somehow disabled, first disable the EWF (Enhanced Write Filter), and then set the service to run Automatically.

Reboot Windows (from the start menu) and confirm if the touch screen now works.
Was this helpful?
What can we do to improve the information ?