Browse FAQs

What is the wire torque value for 8903L power lugs?

Published date: 14 May 2019

Issue:
What is the torque value for 8903L power lugs?

Product Line:
8903 Type L and Type LX, Lighting Contactors

Environment:
all

Resolution:
The recommended torque for the power terminals is 20 lb-in (2.26 N•m).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.