Browse FAQs

PM55xx series firmware Version 2.7.4 and release notes

Published date: 14 May 2019

Issue
Looking for new firmware upgrade

Product Line
PM5500 series meter

Environment
Firmware Upgrade

Cause
Need to upgrade PM5500 series meter to the latest firmware version

Resolution
Release Notes: PM55xx firmware upgrade to address new and updated features for firmware version 2.7.4.

Updates: This version implements DNP3 protocol support over Ethernet and selection for the PM5563 for the PM5RD hardware version.

Note: This firmware update is intended for PowerLogic PM5560 and PM5563 meters.

Please see the following link for more information regarding PM5560 / PM5563 V2.7.4 Release

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.