Browse FAQs

What is the recommended cable type to be used with the ATV660 drives?

Published date: 07 May 2019

 Issue:
Customer wants to know if they should use 2000V cables or 1000V/600V cables for long cable distances. 

Product line:
Altivar Process, ATV630, ATV930

Environment:
all

Cause:
Long motor cable distance

Resolution:
The type of cable used depends on the length of the cable and the motor selection. 
Each type or brand of wire will have different characteristics (insulation, coupling capacitance, etc). 
Consult the cable manufacturer for selection recommendations.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.