Technical FAQs

Ask a Question

Error AL539 when running LXM28

Issue:
Getting error AL539 when running LXM28

Product Line:
LXM28
Lexium 28

Resolution:
AL539 could appear when we are asking the BCH2 motor to run at a higher speed than it can support
Was this helpful?
What can we do to improve the information ?