Technical FAQs

Ask a Question

Does the Magelis line of HMI support BacNet natively?

Issue:
Does the Magelis line of HMI support BacNet natively?

Product Line:
Vijeo Designer, EcoStuxure Operator Interface Expert, Magelis


Resolution:
Currently none of the Magelis HMIs programmed with Vijeo Designer or EcoStruxure Operator Interface Expert support the BacNet protocol natively. We recommend to use the Modbus protocol in the HMI application and maybe use a Modbus to BacNet converter device like the one below:
https://www.sierramonitor.com/ez-gateway-modbus-bacnet

 
Was this helpful?
What can we do to improve the information ?