Technical FAQs

Ask a Question

Is the ION8650 compatible to save waveform data in COMTRADE format?

Issue
Is the ION8650 compatible to save waveform data in COMTRADE format?

Product Line
ION8650

Environment
Waveform data (COMTRADE format)
ION Setup

Cause
Can the meter provide waveforms in COMTRADE format?

Resolution
Only the ION8650A meters can save waveform data in COMmon Format for TRAnsient Data Exchange (COMTRADE) format, which is then available for download via FTP. THis is intended for use in conjunction with IEC 61850 and is only available on ION8650A meters with an Ethernet port.
Was this helpful?
What can we do to improve the information ?