Technical FAQs

Ask a Question

What are the part reference of cable to connect permium racks to an M580 rack?

The following types of X Bus cables can be used to connect Premium racks to an M580 rack:

Part Number Available Lengths
BMX XBC ••0K 0.8 m (2 ft, 7.5 in), 1.5 m (4 ft, 11 in), 3 (9 ft, 10 in), 5 (16 ft, 4 in), 12 (39 ft, 4 in)
TSX CBY •••K 1 m (3 ft, 3 in), 3 m (9 ft, 10 in), 5 m (16 ft, 4 in), 12 m (39 ft, 4 in), 18 m (59 ft),
28 m (91 ft, 10 in)
TSX CBY 380K 38 m (124 ft, 8 in)
TSX CBY 500K 50 m (164 ft)
TSX CBY 720K 72 m (236 ft, 2 in)
TSX CBY 1000K 100 m (328 ft, 1 in)

NOTE: If you install TSX CBY •••K cables, only use PV 03 or later.
Was this helpful?
What can we do to improve the information ?