Technical FAQs

Ask a Question

What is the IP degree of protection BMXNRP0200/BMXNRP0201?

IP degree protection  BMXNRP0200/BMXNRP0201 is IP20.
Was this helpful?
What can we do to improve the information ?